Browse
STMicroelectronics Community
FAQs
Sign In
Product forums
STM32 MCUs
STM32 MCUs products
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
STM32 MCUs Other solutions
STM32 MPUs
STM32 MPUs products
STM32 MPUs Boards and hardware tools
STM32 MPUs Software development tools
STM32 MPUs Embedded software
STM32 MPUs Solutions
MEMS and sensors
MEMS (sensors)
Imaging (sensors)
Automotive & Transportation
Microcontrollers
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
RPers
Associate II
since
2019-08-06
2023-06-14
User statistics
5
Posts
0
Solutions
0
Kudos given
0
Kudos received
STMicroelectronics Community
About RPers
Options
Report User
User Activity
Posts
Replies
Hello, I have implemented the code for the USB VCP, but when debugging the code the "pdev->pClassData" is always null (0). Where is this class initialized? code line : USBD_CDC_HandleTypeDef *hcdc = (USBD_CDC_HandleTypeDef *)pdev->pClassData;
2020-04-17
Cube MX 5.6.1 generated code:void MX_USB_DEVICE_Init(void){ /* USER CODE BEGIN USB_DEVICE_Init_PreTreatment */ /* USER CODE END USB_DEVICE_Init_PreTreatment */ /* Init Device Library, add supported class and start the library. */ if (USBD_Init(&h...
Re: Hello, I have implemented the code for the USB VCP, but when debugging the code the "pdev->pClassData" is always null (0). Where is this class initialized? code line : USBD_CDC_HandleTypeDef *hcdc = (USBD_CDC_HandleTypeDef *)pdev->pClassData;
2020-04-19
Thanks I noticed that there seems to be a delay.I will give it a shot.Rex
Re: Hello, I have implemented the code for the USB VCP, but when debugging the code the "pdev->pClassData" is always null (0). Where is this class initialized? code line : USBD_CDC_HandleTypeDef *hcdc = (USBD_CDC_HandleTypeDef *)pdev->pClassData;
2020-04-19
Yes I do have FreeRtos implemented.Thanks for the hintRex
Re: Hello, I have implemented the code for the USB VCP, but when debugging the code the "pdev->pClassData" is always null (0). Where is this class initialized? code line : USBD_CDC_HandleTypeDef *hcdc = (USBD_CDC_HandleTypeDef *)pdev->pClassData;
2020-04-19
Thanks PavelRex
Re: Hello, I have implemented the code for the USB VCP, but when debugging the code the "pdev->pClassData" is always null (0). Where is this class initialized? code line : USBD_CDC_HandleTypeDef *hcdc = (USBD_CDC_HandleTypeDef *)pdev->pClassData;
2020-04-18
Thanks for the reply. I will look into thisRex