cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, I have implemented the code for the USB VCP, but when debugging the code the "pdev->pClassData" is always null (0). Where is this class initialized? code line : USBD_CDC_HandleTypeDef *hcdc = (USBD_CDC_HandleTypeDef *)pdev->pClassData;

RPers
Associate II

Cube MX 5.6.1 generated code:

void MX_USB_DEVICE_Init(void)

{

 /* USER CODE BEGIN USB_DEVICE_Init_PreTreatment */

  

 /* USER CODE END USB_DEVICE_Init_PreTreatment */

  

 /* Init Device Library, add supported class and start the library. */

 if (USBD_Init(&hUsbDeviceFS, &FS_Desc, DEVICE_FS) != USBD_OK)

 {

  Error_Handler();

 }

 if (USBD_RegisterClass(&hUsbDeviceFS, &USBD_CDC) != USBD_OK)

 {

  Error_Handler();

 }

 if (USBD_CDC_RegisterInterface(&hUsbDeviceFS, &USBD_Interface_fops_FS) != USBD_OK)

 {

  Error_Handler();

 }

 if (USBD_Start(&hUsbDeviceFS) != USBD_OK)

 {

  Error_Handler();

 }

 /* USER CODE BEGIN USB_DEVICE_Init_PostTreatment */

  

 /* USER CODE END USB_DEVICE_Init_PostTreatment */

}

to send data this is implemented

 while (1)

 {

  /* USER CODE END WHILE */

 USBD_CDC_SetTxBuffer(&hUsbDeviceFS, &buffer[0], sizeof(buffer));

 USBD_CDC_TransmitPacket(&hUsbDeviceFS);

 HAL_delay(1000);

  /* USER CODE BEGIN 3 */

 }

This discussion is locked. Please start a new topic to ask your question.
8 REPLIES 8
Pavel A.
Super User

> Where is this class initialized?

pdev->pClassData is initialized when you call USBD_RegisterClass.

If it is 0 after successful return from USBD_RegisterClass, you probably have memory corruption.

-- pa

Thanks for the reply. I will look into this
Rex
TDK
Super User

This field is only populated after the PC successfully enumerates the device, which is not instant. It also uses malloc, which is probably not what one would expect.

Typically putting HAL_Delay(500) prior to using the USB functions works, although it's not an elegant solution.

If you feel a post has answered your question, please click "Accept as Solution".

Please see here for example (STM32F0). No allocation, and the pointer to the class struct is stored immediately.

Here is shown how USBD_RegisterClass is called.

-- pa

chaaalyy
Senior II

If you use freeRTOS, also take a look here (in case of memory corruption...) :

http://www.nadler.com/embedded/newlibAndFreeRTOS.html

Thanks Pavel
Rex
Yes I do have FreeRtos implemented.
Thanks for the hint
Rex
RPers
Associate II
Thanks I noticed that there seems to be a delay.
I will give it a shot.
Rex