User Activity

Hi, I'm working on an OTA BLE bootloader for the STM32WB5MM module.I created from scratch with STM32CubeMX the same code as the OTA example for NUCLEO-WB55.I'm on BLE stack 1.21So far so good, I can update with the smartphone app.The problem I'm havi...
Hello, I'm trying to do a quick test with the STM32F412G-Discovery kit and the analogue microphone input.I use this example https://github.com/STMicroelectronics/STM32CubeF4/tree/master/Projects/STM32F412G-Discovery/Examples/BSPwith the menu #### AUD...
Hello, I'm testing the STM3240G-eval with the USB host MTP. The goal is to retrieve the photo from a canon EOS 100.The camera uses PTP protocol.As the demonstration  code read .wav file, I wrote a wav file to the root of the SD card. The digital came...
Hello,In a Client(Router)/Server configuration with two STM32WB55 I would like to accelerate the transmission of data at starting of the server.The server address is know in advance and stored in the client then in the HCI_LE_ADVERTISING_REPORT_SUBEV...
Hello, I'm using the client/server example with two Nucleo-WB55 kit, it works without issue.Now I'm working with my own board:Client : STM32WB5MM moduleServer: the same nucleo-WB55 as above At starting, the client scans and detects the server(with th...
Kudos from
Kudos given to