User Activity

Hi all,I want to connect an STM32H573 device to a LAN8742A to create an Ethernet interface.Is there any board hardware guidelines available for this ?The LAN8742A is used in REF_CLK OUT mode (50 MHz clock output from the PHY routed to the RMII_REF_CL...
Hi,The datasheet of STA8090FG only list in table 5 the test/emulated dedicated pins but there is no information how to use the pins.Is it IEEE 1149.1 compliant ?What are the interface timings ?Does TRSTn only reset the JTAG logic and must be left to ...
Hi,Is it possible to change of pin usage ?For an application we do not have the use of I²C link (SDA,SCL pins) and Wake-up or Ant_OFF pins. (only UART interface would be useful)Can those pins be configured as GPIO ?Thanks