2019-06-17 9:29 AM
Hi,
The datasheet of STA8090FG only list in table 5 the test/emulated dedicated pins but there is no information how to use the pins.
Is it IEEE 1149.1 compliant ?
What are the interface timings ?
Does TRSTn only reset the JTAG logic and must be left to ground during normal operation ?
Thanks,
Regards.
2019-06-17 9:39 AM
I'd imagine it functions like the JTAG on every other ARM9 based core from the last few decades. Pretty sure the eval board exposes it to a header, and has a schematic.
https://www.st.com/resource/en/data_brief/dm00373428.pdf
Doesn't Thales have a business account and contacts directly into ST they could use to find an FAE? They'd probably be able to supply an IBIS file too.