User Activity

Two days ago, SDCC 4.4.0, a C compiler targeting various 8-bit architectures, including STM8, was released. IMO, for the ST8, the main two improvements over SDCC 4.3.0 are:New optimizations, in particular generalized constant propagation and the rota...
There is now a Release Candidate 1 for the 4.3.0 release of the Small Device C Compiler (SDCC), a free ISO C compiler targeting the STM8 and other 8-bit architectures.Source, documentation and binary packages for amd64 Windows, amd64 macOS and amd64 ...
There is now a Release Candidate 1 for the 4.3.0 release of the Small Device C Compiler (SDCC), a free ISO C compiler targeting the STM8 and other 8-bit architectures.In addition to the source package, binaries are available for x86 and amd64 Windows...
I wonder why some developers choose non-free compilers (IAR, Cosmic, Raisonance, etc) instead of the Small Device C Compiler (SDCC) when targeting the STM8.
This is not a question, so it doesn't really belong here, but the community forum is still broken, so there is no other place to post this.I just redid my comparison of the 4 most important STM8 C compilers (previous comparisons were in 2016 and 2018...
Kudos from