2019-03-27 10:33 PM
The B-L475E-IOT01A contains the spsgrf-915 module. I want to use this without an extension board to run FP-NET-6LPWIFI1. Is it possible? It is necessary to refer to it if possible.
Solved! Go to Solution.
2019-04-07 8:38 PM
Well, it is certainly possible to run FP-NET-6LPWIFI1 wifi-bridge application with SPSGRF-915 instead of X-NUCLEO-S2868A1.
Unfortunately, currently this package is implemented with X-NUCLEO-S2868A1 only.
Since X-NUCLEO-S2868A1 is based on S2-LP and SPSGRF-915 is based on SPIRIT1, modifications will be required to make the application work with SPSGRF-915.
Please refer to the FP-SNS-6LPNODE1 package, search for 'X_NUCLEO_S2868A1' in comparison to 'X_NUCLEO_IDS01A5'
and also 'SPIRIT1_RADIO' in comparison to 'S2LP_RADIO'.
Hope it helps.
2019-04-07 6:25 PM
Hi shk,
Are you looking for a 6LoWPAN package for Sub-1GHz modules instead of WiFi?
Please try FP-SNS-6LPNODE1 instead, which will work with SPSGRF-915 module directly.
Best Regards,
Winfred
2019-04-07 7:32 PM
Thank you for your answer.
There was a mistake I did not specify the question.
I would like to run the [fp-net-6lpwifi1] -> [wifi-bridge] application using only the B-L475E-IOT01A Board (B-l475e-iot01a board includes wifi module and spsgrf-915 module).
However, the example is based on the B-L475E-IOT01A + X-NUCLEO-S2868A1 expansion board.
2019-04-07 8:38 PM
Well, it is certainly possible to run FP-NET-6LPWIFI1 wifi-bridge application with SPSGRF-915 instead of X-NUCLEO-S2868A1.
Unfortunately, currently this package is implemented with X-NUCLEO-S2868A1 only.
Since X-NUCLEO-S2868A1 is based on S2-LP and SPSGRF-915 is based on SPIRIT1, modifications will be required to make the application work with SPSGRF-915.
Please refer to the FP-SNS-6LPNODE1 package, search for 'X_NUCLEO_S2868A1' in comparison to 'X_NUCLEO_IDS01A5'
and also 'SPIRIT1_RADIO' in comparison to 'S2LP_RADIO'.
Hope it helps.
2019-04-07 9:09 PM
Thank you. I'll try.