Posted on May 17, 2011 at 09:56Hello, How create a digital toggle signal on GPIO4 for the STR9-comstick ? I create it but the maximum frequency is 300KHz with jitter on the signal. There is a way for higher frequency ? regards
Posted on May 17, 2011 at 09:56Hello, Thanks for your answer. i don't want to program ARM processor in VB but control the code in the ARM processor by VB. My final project is to program a sequence acquisition for an extern ADC board connect to STR9-...
Posted on May 17, 2011 at 09:56Hello, I develop an application with the STR9-Comstick. The idea is to control the I/O ports with a program in Visual Basic through the USB-B connector near the pins of I/O ports. Which dll use for that for the enumera...
Posted on May 17, 2011 at 09:51Hello, I develop an application with the STR9-Comstick. The idea is to control the I/O ports with a program in Visual Basic through the USB-B connector near the pins of I/O ports. Which dll use for that for the enumera...
Posted on May 17, 2011 at 09:35Hello, I develop an application with the STR9-Comstick. The idea is to control the I/O ports with a program in Visual Basic through the USB-B connector near the pins of I/O ports. Which dll use for that for the enumera...