User Activity

Hi all,I want to run an application to record audio from the microphone, as here is said:https://www.youtube.com/watch?v=QIPQOnVablYbut my Cube doesn't have any options for DAC, there is only ADC1. For pin PA4, which should be DAC_OUTPUT, I have only...
Hi,I have a problem with connecting my STM32 F4 Discovery to USB. I use Eclipse with CubeMX and I configured USB as Device_Only, VBUS_activate and the rest I left as default. I also set in USB_DEVICE the Class for FS IP "Communication Device Class (V...