User Activity

Hi,I would like the DC/DC converter of STKNX to make 5V.Also, I want the Linear regulator to make 3.3VBecause of global efficiency, I wanted to power the linear regulator with the 5V output of DC/DC converter.I'm surprised that the datasheet specifie...
Hi,I'm using STSPIN220 to drive a stepper motor with a pushrod.I only using full step mode, in order to have max. torque.I would like to detect when pushrod gets in contact with some item (increase torque), and also if stall/blocking.what would be th...
Hi everyone,On my system, there is cloud station backup working in background, so each file that is modified is back-up on distant synology server.This works very fine...Problem is, if starting code generation of STM32CubeMX, code generation starts a...
Hello everybody,On actual project, I need to interface my STM32F051C8 to a HTS221TR Temperature & Humidity sensor.Communication is through SPI1, STM32 is master, there is 1 bidirectional data line, 1 clock, 1 Slave Select.Final usage will be in polli...
Kudos given to