I did also try to recover files via recuva, but I got garbage too. In my case it was nVidia driver who overwrite sector. I hope you find a way to recover project. There are numerous people with the same issue. ST should listen to users and resolve th...
Hope you have backup. Do not restart computer, create a project folder with identical name as your lost project, inside create main.c file, then go to file history tab in windows explorer and check if windows backed up your main.c. This only works wi...
Hi Markus, check my problem here.https://community.st.com/s/question/0D50X0000Ap1NYTSQ2/bug-stm32cubeide-deleted-all-my-source-code-generate-code-on-imported-projectI did uninstal 1.7.0 manualy and then tried to build solution. IDE (1.0.2) then asked...
Yes this happened to me. 2 month of work until I figured out that even Acronis did not backed up even once in 2 months so I lost everything. Is there a solution to get back code? I migrated from 1.0.0 to 1.0.2 but then I got error Upgraded to 1.0.2, ...