Hello @rbmarcus,I have analyzed your project. Unfortunately there is an issue in MEMS Studio in saving the labeled data in Data Analysis tool. This caused data corruption and the logs cannot be process by the AFS tool.A workaround could be split the ...
Hello @mariagragna,Yes, it possible to acquire the raw QVAR signal using only MEMS Studio and DatalogExtended firmware.First of all you have to configure the X-NUCLEO-IKS01A4 to connect the electrodes to the LSM6DSV16X. The configuration is described...
Hello @AlexJ this is definitely different issue. The error you see is only warning and doesn't have any impact.I'm not able to replicate it. Didn't you do any modification in the boards?I would recommend you to use MEMS Studio instead of AlgoBuilder...
Hello @StephanMP,the waring is expected it is due to a new feature in gcc compiler, you can ignore it.I was able to replicate your issue are there is a bug in the firmware, we will fix in next release of MEMS Studio.In the meantime you can add __HAL_...
LIS2DUXS12 is sharing the QVAR with INT pins and on the X-NUCLEO-IKS4A1 are these pins connected to level shifter. So the QVAR functionality cannot be used.