User Activity

I build a project in the CubeIDE (program-project). Late i decide to make some Test for this project in another project(testing-project). Know i want when i build the testing-project, that it directly take the sourcefiles from the program-project. So...
Hello erverbody,I had a Projekt, build with FreeRTOS and Ac6 plugin and Eclipse.Know I try to figure out if the stack size of the task is set correctly.For this i generate the .elf file and the .su file with the eclipse/Ac6 setup.Is there a way to lo...