Hi everyone, I am trying to read ADC values from 4 different channels PC0 ------> ADC1_IN1 PC1 ------> ADC1_IN2 PC2 ------> ADC1_IN3 PC3 ------> ADC1_IN4I am able to get different values from different channel for the 1st iteration. but from th...
I have checked all the required positions of the jumpers on the STM32 Nucleo board as follows: • JP1 - USB STL • JP2 ON • JP3 ON I have installed Java 8. I have selected ST-Link mode, the device is visible in device manager as STLink Virtual PortI al...
hello, Iam having a issue in uploading the code to STM32F100ZC, I have attached the schematic of SW interface done. Its showing an error that target is not connected. I have done all the possible connections for BOOT0 and BOOT1 pins.Please h...
Thank you so much for replying.all the jumpers are installed correctly, I have rechecked. Yes the target seems to be powered properly with the mini-USB cable.Could you please elaborate what is reset mode configuration in ST-LINK?Thank you in Advanc...