cancel
Showing results for 
Search instead for 
Did you mean: 

BlueNRG-LP (STEVAL-IDB011V1) not detectec by BlueNRG GUI v4.0.0

pixel
Associate II

My evalboard seems to work. (I can flash the demo projects)

But when I try to use the GUI, it does not detect the device. "No Firmware detected on motherboard..."

It is successful to flash the Firmware STEVAL-IDB011V1/USB_CMSISDAP.hex but afterwards everything starts from the beginning.

What can I do?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
pixel
Associate II

Solved:

Did a clean step by step flash again. Now it works as expected:

Hold Reset, Plug USB, Maintenance Mode -> USB_CMSISDAP.hex

Drag&Drop -> DTM_UART_WITH_UPDATER.hex

BlueNRG GUI Update -> DTM_UART_FOR_UPDATER.bin

Had to remove JP5 for the first / second step. Do not remember.

Got an error before: error: The interface firmware FAILED to reset/halt the target MCU type: target

View solution in original post

1 REPLY 1
pixel
Associate II

Solved:

Did a clean step by step flash again. Now it works as expected:

Hold Reset, Plug USB, Maintenance Mode -> USB_CMSISDAP.hex

Drag&Drop -> DTM_UART_WITH_UPDATER.hex

BlueNRG GUI Update -> DTM_UART_FOR_UPDATER.bin

Had to remove JP5 for the first / second step. Do not remember.

Got an error before: error: The interface firmware FAILED to reset/halt the target MCU type: target

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.