I have a STM32F3DISCOVERY, STM32CubeIDE, Windows11.After writing the program to STM32F3DISCOVERY and turning on the debug and canceling the break, I still have to do a RESET. Is it possible to set STMCubeIDE so that I do not have to RESET?
Please link to the schematic. Is there any input with a pull-up resistor up to 5V?Please link to the schematic. Is there any input with a pull-up resistor up to 5V?
Error in final launch sequence:Failed to execute MI command:target remote localhost:61234Error message from debugger back end:localhost:61234: Connection timed out.Failed to execute MI command:target remote localhost:61234Error message from debugger ...