Hello,I try to do a connection via TCP with LWIP/FreeRTOS activated (ioc file joined)For testing i use telnet command and I am unable tio pass the "accept" function.Here the simple piece of code: int sock, newconn, size; struct sockaddr_in add...
Hello,I'm independent developer involved in a STM32H7 project.I need to activate traces in SWV console of TrueSTUDIO. I've attached my .io CubeMX project, I think it is well configured.I've configured in the debugger tab of TrueStudio : SWD // SWV ch...
Hello,I've searched all the day and read a lot of posts and it was very helpful. I think I have all configured at best but something remain wrong and it's for that reason I have poste my ".io" file.If someone can help me I'll really appreciate.