Posted on May 17, 2011 at 13:22Hi everybody! is ST planing a STM32 processor with an integrated ethernet PHY+MAC??? I ask you because I think that the STM32 is a little too expensive vs. the Cortex M3 processors of Luminary if you want to use ether...
Posted on May 17, 2011 at 13:09Hi! I've 4 STM32 processors on my board that are all connected on the boot0 pin with each other without a series resistor. This common boot0-signal is set or reset by another microcontroller and so I can select the bo...
Posted on May 17, 2011 at 13:09You can also generate 5V output signals with the STM32: configure a 5V-tolerant pin as open drain and use it in conjunction with an external pull-up resistor.