cancel
Showing results for 
Search instead for 
Did you mean: 

Boot0 internal connection

walterma
Associate II
Posted on April 14, 2009 at 11:24

Boot0 internal connection

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
walterma
Associate II
Posted on May 17, 2011 at 13:09

Hi!

I've 4 STM32 processors on my board that are all connected on the boot0 pin with each other without a series resistor. This common boot0-signal is set or reset by another microcontroller and so I can select the boot mode (boot1 is pulled down with a 10k resistor). Now, I've to calculate a series-resistor for this common boot0-signal. How is the boot0-pin configured at startup?? are the pull-down or pull-up resistors activated??

Thank you very much!!