After using STM32F417VGT6 chip, PA11 PA12 is configured as USB HOST (non-OTG mode, HNP or SRP mode is not used), PA9 cannot be configured as input pull-up mode; without USB HOST, PA9 can be configured as input pull-up Yes; try to configure PA9 to out...