STM32CubeMX allows only Full HS for STM32H7B3VIT. According to the datasheet, that 100 pin derivate do have a support for HS and external PHY (ULPI). Please, advice, if the 100 pin supports ULPI or how to setup it in the STM32CubeMX.
Please, if you can answer also the following:Does the same limit to ULPI and 100/144 packages apply to STM32H7B0, STM32H7A0 and other STM32H7 members ?When will members in WLCSP132, LQFP176 and UFBGA169 be available ? Will they be avaialble for sma...
Thanks. However, before we put an effort and decide for PCB layout, I would need to know exactly and directly from ST, if that ULPI feature is supported on 100 (and 144 as well) pin derivates of STM32H7B3 or not. Also, when STM32CubeMX support can be...