User Activity

Hi,I am using STM32CubeMX, ver 6.1.1 on Linux and I noticed the following bugs in the Makefile generation:The first problem: The C_INCLUDES variable.--------------------------------------------------------------If a Makefile does not exist in the tar...
Hi,Based on AN4872, I managed to get the id, version, erase, read and write memory commands working. I'm able to erase the entire flash of a BRNG-M2SA or BNRG-M2SP and write a pre-built example bin file to the flash and read it back, without errors.H...
Hi,Compilation of the BlueNRG-1_2 DK 3.2.1 on Linux fails due to two files that were misspelt. The spelling mistakes are due to the fact that Windows file systems are not case sensitive and explains why it compiles on Windows, but not on Linux.For th...
Hi,I'm trying to update the FW of the BLUENRG-M2SP module on my X-NUCLEO-BNRG2A1.I'm using CubeMX with the X-Cube-BLE2.3.1.0 SW pack, together with the IFRStackUpdater application. The IFRStackUpdater works perfectly up to the point where the "Blue F...
Kudos from
Kudos given to