Posted on May 17, 2011 at 11:32Hi, im configuring SSP0 as a slave in MCB-STR912 board, could i connect SSP0_MISO to SSP0_MOSI to see the loopBack effect on the oscilloscop without damaging the chip as the soft loop back seems not working and i can n...
Posted on May 17, 2011 at 09:56hello, i have set SSP1 as a slave in my MCB-STR9 board, when i send the data i get FF on Pin 3.5 i SSP_Cmd(SSP1, ENABLE); while(1) { SSP_SendData(SSP1, 0x3A); } should i add some thing plz help
Posted on May 17, 2011 at 09:53hello, we are using SPI port as a master connected to onother MCU should we use pull up resistors in between because the signal could be visualized in oscilloscop without connection once we connect SPI master to slave ...
Posted on May 17, 2011 at 09:52Hi every body, is it possible to connect STR912 I/Os to low voltage CMOS interface (exemple SPI), and TTL interface (exemple UART),please advise :)