Hello Oliver,STM32WB05 is rebranding of BlueNRG-LPS.This are exacting same devices, meaning the FW you have developed for BlueNRG-LPS will run on your STM32WB05.STM32WB0x series comes with a different ecosystem (SDK and tools) versus BlueNRG, here is...
Yes I see.My request is maybe to rebuild FW with DIO7 as IRQ and modify your PCB as a test.DIO7 is the default IRQ used in our example.This is to see if this is related to DIO14 and any specifc thing around it. Laurent
Hi, No more idea on my side.May be could you confirm using DIO7 as IRQ as our default example, you can see IRQ rising up (you can add wire to modify your PCB)? Laurent
Hello, On BlueNRG-M2SA, 32kHz is used and SMPS is implemented so you must definedLS_SOURCE=LS_SOURCE_EXTERNAL_32KHZSMPS_INDUCTOR=SMPS_INDUCTOR_10uHSee DT037 documentation. Laurent
Hello, Can you try below :- Do a full mass erase- Flash the DTM SPI no updater version you will have rebuilt but having set MEMORY_FLASH_APP_OFFSET=0x0 instead of 0x2000 in the linker optionRegardsLaurent