Hello detakm,I'm facing the same issue since months. I was able to have both BLE and Zigbee with older stacks and a lot of efforts, without FreeRtos. I hardly remember if they finally worked with FreeRtos.The last stacks (autumn 2021 1.13.1) were sup...
Hello, sure, if persistence (as ST examples) or similar (Zigbee network parameters) with ZbRejoin behavior, this not happening. I had the time to add this feature, works well,Such security protections are mandatory, but could be annoying at first for...
Bonjour,I use 2 different endpoints (one for sensors, the second for a relay). The Basic cluster is embedded twice, that's the default as you written..Please note : The ZbZclAddEndpointNoBasic function appears in the zcl.h file, but is not defined. ...
Hello,I have this behavior daily during my design phase : ZB_APS_STATUS_SECURITY_FAIL during join.Each time a restart the software to test, I can't join the network, because the node previously joined it during the last debug session.I have to :power...
Hello,I'm reusing this thread, as I encounter similar problems.Without initialization, the Basic cluster contains "ST" values.I'm able to update the Basic cluster attributes with ZbZclBasicWriteDirect, once the endpoints are created. Values are shown...