User Activity

In a custom design using a STM32H733vgt and a USB3318 phy, operating as a virtual com port device, full-speed works but high-speed doesn't work. If full-speed works but high-speed doesn't, what do you think would be the culprit?I'm using virtual com-...
The execute() API starts execution of the application but is there an API to halt, stop or pause execution?The STM32CubeProgrammer GUI has a Halt button...How does the GUI use the API to Halt the CPU?
Posted on April 12, 2018 at 23:49Using the MCSDK 5.0.1, I can startup and run a BLDC motor most of the time. About 10% of the time, I get a Start-up failure and each time I can see from the Motor Control Workbench GUI that the speed has reached the ...
Posted on April 02, 2018 at 20:57I'm attempting to generate project code for the STEVAL-SPIN3202.ST32CubeMX doesn't have an option for the STEVAL-SPIN3202 so I tried using the ST Motor Control Workbench and it gives an error 'STSPIN mcu not supporte...
Kudos from