2022-10-04 3:10 PM
The background is I am trying to build a pass through or charge through dongle like application. Using a G0 with 2 UCPD ports, port 0 as sink, and port 1 as DRP, using the respective TCPP chips
My goal is to have the input port 0, get the available PDO's, subtract the power consumed by the device, then pass these adjusted PDO's to the output, port 1, letting the up stream device chose. Once a PDO is selected on port 1, port 0 would also select the corresponding PDO
I have a couple questions about implementing this with UCPD on STM. I'm just fumbling around with a test project (no HW yet) but I can't seem to see how one would dynamical set PDO's. Specifically:
Can PDO's be set and removed dynamically during run time?
What part of the PD code would be the best area to edit / add this functionality ?
Cheers
Solved! Go to Solution.
2022-10-13 2:46 AM
Hello @Community member ,
I would suggest first to have a look at the following wikis (including the optional sections) in order to have a complete code which is able to handle multiple PDO.
https://wiki.st.com/stm32mcu/wiki/STM32StepByStep:Getting_started_with_USB-Power_Delivery_Sink
https://wiki.st.com/stm32mcu/wiki/STM32StepByStep:Getting_started_with_USB_Type-C_only_Source
Then, you should be able to modify the software to declare PDO dynamically, and handle them accordingly.
In our example applications, PDOs are declared statically in file usbpd_pdo_defs.h. They are declared in arrays, PORT0_PDO_ListSRC & PORT0_PDO_ListSNK.
The section of code that handles the actual PDOs is in the advanced section of the wiki for example for a SNK.
So, yes, you can manage PDOs dynamically, but you will need to modify these sections of code according to your needs to implement this functionality.
Best regards,
2022-10-13 2:46 AM
Hello @Community member ,
I would suggest first to have a look at the following wikis (including the optional sections) in order to have a complete code which is able to handle multiple PDO.
https://wiki.st.com/stm32mcu/wiki/STM32StepByStep:Getting_started_with_USB-Power_Delivery_Sink
https://wiki.st.com/stm32mcu/wiki/STM32StepByStep:Getting_started_with_USB_Type-C_only_Source
Then, you should be able to modify the software to declare PDO dynamically, and handle them accordingly.
In our example applications, PDOs are declared statically in file usbpd_pdo_defs.h. They are declared in arrays, PORT0_PDO_ListSRC & PORT0_PDO_ListSNK.
The section of code that handles the actual PDOs is in the advanced section of the wiki for example for a SNK.
So, yes, you can manage PDOs dynamically, but you will need to modify these sections of code according to your needs to implement this functionality.
Best regards,
2022-10-18 5:42 PM
Thanks @HFISTM
The advanced section is helpful, I see there is a git with a DRP example as well
Cheers
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.