User Activity

Hi, I'm new to this, so bare with me :) I'm following the UM2421 - getting startet guide for the P-NUCLEO-IOM01M1, and everytime I connect the USB to my PC, I get the FAIL.txt where it says: The interface firmware FAILED to reset/halt the target MCU....
The control tool can correctly identify the Imported IODD-file, but when i try to setup the IO-link communication in the control-tool I recieve the COMLOST fault. Furthermore I receive an Event error with the code: 49415. The STEVAL-IOM001V1 is corre...