HI, After Factory calibration of LIS3DH accelerometer, what are the range of values given by the accelerometer( Selected 12 bit OUTPUT). I am getting 20-30 ADC counts of X axis from accelerometer, where as -1 to 3 counts from Y axis . Why there ...
HI,In LSM3DH accelerometer sensor datasheet given output of accelerometer is 16 bitthey are divided into two 8bit registers. MSB, LSB registers. LSB register is always giving ZERO as output. only MSB register is giving output.Why LSB register is alwa...
I want to use an accelerometer to calculate the speed of a moving vehicle. For this i need a accelerometer which should give _ve values(2's complement) in Deceleration and +ve values in (2's complement) in acceleration. It should have 2g range with 1...
Dear, I am trying to find speed of a moving vehicle using accelerometer. Is there any acclerometer with you(ST) ? Please Suggest me one. If any body done with this Project, please Share your Experience.Thank You.
Greetings, @Community member &@Eleon BORLINI In data sheet of LIS3DH accelerometer , they have given that output is 16 bit and it has two 8bit registers. But the LSB register always giving me output as ZERO. only...
@Community member Your answer is not relevent to my question. Please check my question once. i am asking about the values given by sensor in deceleration.please read total convesation and answer my doubt.Please help me.
Greetings, I want to calculate speed from acceleration, I have to integrate the acceleration data, means every time i have to add the samples of the axis which was parallel to the ground (not affected by Gravity of earth). It was not...
Greetings, In TESEO_DRAW they are using ODOMETER. I want to find the speed without ODOMETER, with only accelerometer or IMU sensors.Please answer my doubts.