User Activity

Hello, i just installed CubeIDE / MX on a brand new Computer. I am running Windows 11.Both IDE and MX have a problem with downloading "software packages" The are extremly slow and after an hour i get an error message. I am not able to work with that ...
Hello, i am struggling with creating an working image of my openblt bootloader and my user application.When i just flash the bootloader, and upload the user application via bootloader pipeline everything works fine.But when i try to use srec_cat  or ...
Hi, i have a simple bootloader and a application on top. Both works fine so far. But after the implemented the bootloader my UART2 is not working anymore. so no output.When i remove the bootloader (change linker file and system... file) UART function...
Hello everybody,i am having trouble determining the wakeup source after power cycling and i can not figure out why this is.Simple test case:I am using the NUCLEO-L496ZG->Examples->PWR->PWR_SHUTDOWN example as a base.The example was slightly modified ...
Hello,i tried to implement a I2C slave device on a STM32L486.It is working, but sometimes (after a few seconds, minutes or even hours) it freezes/blocks the SCL line. So the master device (also a STM32) generates a error.I have no glue what happens h...
Kudos from