cancel
Showing results for 
Search instead for 
Did you mean: 

Multi-channel SDADC on STM32F373 using HAL

EA50
Associate

This question was asked but it is now closed , so i want to ask again

If some one can share code of how to do sdadc3 for multichannel via

  1. DMA |
  2. ISR |
  3. interrupts |

preferred DMA

All code example shows how to work with single channel.

The reason i am asking is that  because i tried with DMA and i cannot find any configuration

that DMA start will accept.

it looks to me that SDADC in F373 works only with one channel.

i need the row values from the ADC.

Thanks!

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
User.119
Associate

I also need this part of the sample program, but there is no answer.