Yes, it works!But there is one feature.The "Power Regulator Voltage" (System Core, RCC) was in "Power Regulator Voltage 1" mode after setting the clock frequency to 400 MHz.If I change the frequency to 200 MHz, then the Cube automatically calculate t...
Sorry I'm a newbie in STM32 and may misunderstand the acronyms. If it's register PWR_D3CR_VOS, then VOS_0 = 1 and VOS_1 = 1. I have "DevEBox" development board. ST-LINK conntect by SWD mode.