User Activity

I tried the BSP example for H735G-DK, but it doesn't work.What I want to do is get an audio wave from line_in (the blue audio jack on the board).The setup for SAI1 is in the picture, I can play the audio through the line out without any problem but c...
I'm using CubeMX to generate the start file rather than the BSP example. When I tried to set the DMA2D, I found that the start address will be shifted by 0xC.... // setup octospi2 for hyperram, dma2d and ltdc above uint32_t col; uint32_t startAdd = 0...
I was trying to read the 24AA64FT EEPROM using the I2C DMA methods. But the I2C read will break after reading 2 bytes for no reason, and both SDA and SCL stay low. As you can see in the picture, the reading starts with writing 0x50 (0xA0 >> 1) to the...
Kudos from