User Activity

Hello!I have multiple LIS2DS12 accelerometers; according datasheet, it is possible to get data rate high as 3200 and even 6400 Hz. In both cases there are built-in filter with 1420 or 2840 Hz cutt-off frequency. As this accelerometer have internal mu...
I need to know routin to use multiple LIS2DS12TR on one SPI if it's possible. If I undestood correctly nCS pin used to selecting between I2C and SPI mode. So if CS is high, SDO is open-drain. Is I need to simply connect SDO pins of LIS2DS12TR (may ...