>> You mean Detect Pin right?Yes>> I just view the website you provide,it seems a little bit different with mine,but still Appreciate.>> I`m wondering if there any example or method can give me some advises.CUBE MX generates the wrong code for proces...
in the option FATFS -> PLATFORM SETTINGS do not forget to set the input pin, which is responsible for the installed memory card, otherwise the initialization will fail (0 - there is a memory card, 1 - no)