Posted on February 28, 2017 at 16:221:I have developed a small program for the STM32L031 Nucleo-32 using the example UART_TwoBoards_ComIT. The program run on the STM32L031 Nucleo-32 develop-board. When I load* the program to our own HW it does not s...
Posted on February 09, 2017 at 11:00Hi I need a target file (*.STmap) for downloading the STM32L031G6 using the 'Flash Loader Demonstrator' V2.8.0. I only got STM32L0_x3_x2_x1_64K.STmap, but STM32L031G6 is only 32K.
Posted on March 02, 2017 at 08:48Hi CliveFYI1: I forced the program to use the HSE clock now it works.2 The TDO_SWO is optional now the bugger also works.Problems solved!-Mads
Posted on March 01, 2017 at 10:13Hi CliveI understand I can't use the SWIM connector, but what about TDO_SWO connection?ST-LINK/V2connector(CN3)ST-LINK/V2 functionTarget connection(JTAG)Target connection(SWD)STM32L0311,2VAPPTarget VCCMCU VDD(1)MCU V...