cancel
Showing results for 
Search instead for 
Did you mean: 

FlashLoader demonstrator for STM32L031G6

Mads Enevoldsen
Associate II
Posted on February 09, 2017 at 11:00

Hi I need a target file (*.STmap) for downloading the STM32L031G6 using the 'Flash Loader Demonstrator' V2.8.0. I only got STM32L0_x3_x2_x1_64K.STmap, but STM32L031G6 is only 32K.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Khouloud GARSI
ST Employee
Posted on February 09, 2017 at 16:43

Hi

enevoldsen.mads

,

A release candidate of the STMFlashloader (V2.9.0) was previously shared underthis

https://community.st.com/0D50X00009XkYU8SAN

. It supports your device.

The official release will be soon available on ST website.

Khouloud.