User Activity

Hi there,I have 2 modebus register 0x0010, 0x0011. These are enable encryptionkey value. There square vaule should be less then 255 for some reason. This modebus register can be allowed for certain command functions as follows.void ModebusSetCMD_ENE...
Hi there,I am handling a project which has display application both for English and Korean front.I can made some Chineess front/ charecter using Note pad pixel and a software named KSX1001.May be ASCI II can be generate b16*16 PIXEL image file.Now it...
Hi there,I am looking for a customized design where good power solution can be applicable.My aim is to develop a DC-DC sutable toloplogy ( flyback, buck, isolated ,..so on) converter with following parameter, with the idea https://www.smps.us/topolog...
Hi there, I had experience in IAR before, but many of its functionality I dont know well.Currently I am working with customized ST32F103 board.In my F/W code says,Under a function its called,void OnDSP_GetStatus(WORD *pWord){ BOOL bUpdateDSP; float *...
Dear Sir,I have a custom board board with a FW in hand.I am using IAR IDE.What I need to add the output file in configuration and load, run program.Recently I dont have IAR license yet.Could you tell me what to do?
Kudos from