Migration from Linux 4.19 to 5.4 results in a non-booting system
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-01-07 10:41 AM
Hello!
I see many having similar issues, but I have have yet to find a solution to the reason my boot is not happening.
ATF: v2.2-stm32mp-r2.1
U-Boot: 2021.01
Linux: v4.19-stm32mp-r3.3
Works just fine
ATF: v2.2-stm32mp-r2.1
U-Boot: 2021.01 (Edit: and v2020.01-stm32mp-r2.1)
Linux: kernel-stm32mp1-openstlinux-5-4-dunfell-mp1-20-11-12.tar.xz
Results in the kernel outputting the following (LL debug enabled with highest level)
[ 0.398268][ T1] pinctrl core: initialized pinctrl subsystem
...
[ 0.628638][ T1] bus: 'platform': add driver stm32mp157-pinctrl
...
[ 1.831777][ T1] device: 'soc:pin-controller@50002000': device_add
[ 1.838307][ T1] bus: 'platform': add device soc:pin-controller@50002000
[ 1.845361][ T1] PM: Adding info for platform:soc:pin-controller@50002000
[ 1.852543][ T1] bus: 'platform': driver_probe_device: matched device soc:pin-controller@50002000 with driver stm32mp157-pinctrl
[ 1.864472][ T1] bus: 'platform': really_probe: probing driver stm32mp157-pinctrl with device soc:pin-controller@50002000
[ 1.875802][ T1] stm32mp157-pinctrl soc:pin-controller@50002000: no pinctrl handle
[ 1.883752][ T1] platform soc:pin-controller@50002000: Driver stm32mp157-pinctrl requests probe deferral
Then pretty much everything end up with "no pinctrl handle".
I prepared kernel-stm32mp1-openstlinux-5-4-dunfell-mp1-20-11-12.tar.xz by applying all patches and merged the config fragments. My DT is the DK1.
What am I missing?
Edit: I should add that I have tried the ST U-Boot with tag v2020.01-stm32mp-r2.1 with the same result.
- Labels:
-
OpenSTLinux
-
STM32MP15 Lines
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-01-12 7:20 AM
Hi @Community member​ ,
Please confirm we can consider you are now using a consistent V2.1.1 OSTL ?
https://wiki.st.com/stm32mpu/wiki/STM32MP15_OpenSTLinux_release_note#v2-1-1
Between 4.19 and 5.4 dts structure has changed ? Did you align your DK1 DT on the 5.4 structure ?
Else can you share complete boot log ?
Olivier
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-01-13 1:22 AM
I have modifications made to fit my board for ATF and U-Boot in the DT so that should be consistent with your release.
ATF: v2.2-stm32mp-r2.1
U-Boot: v2020.01-stm32mp-r2.1
For the kernel I now took version v5.4-stm32mp-r2.1 (e1b933d696) from https://github.com/STMicroelectronics/linux.git. I build with the
config from board/stmicroelectronics/stm32mp157a-dk1/linux.config and stm32mp157a-dk1 with the following modifications
Debug added to the .config and change of i2c-port for the pmic (if that even matters)
diff --git a/configold b/.config
index d4da5fcc96..6721e130d6 100644
--- a/configold
+++ b/.config
@@ -171,6 +171,7 @@ CONFIG_IO_URING=y
CONFIG_ADVISE_SYSCALLS=y
CONFIG_MEMBARRIER=y
CONFIG_KALLSYMS=y
+# CONFIG_KALLSYMS_ALL is not set
CONFIG_KALLSYMS_BASE_RELATIVE=y
# CONFIG_BPF_SYSCALL is not set
# CONFIG_USERFAULTFD is not set
@@ -683,6 +684,7 @@ CONFIG_DEFAULT_MMAP_MIN_ADDR=4096
# CONFIG_CLEANCACHE is not set
# CONFIG_FRONTSWAP is not set
CONFIG_CMA=y
+# CONFIG_CMA_DEBUG is not set
CONFIG_CMA_AREAS=7
# CONFIG_ZPOOL is not set
# CONFIG_ZBUD is not set
@@ -901,6 +903,9 @@ CONFIG_EXTRA_FIRMWARE=""
CONFIG_WANT_DEV_COREDUMP=y
CONFIG_ALLOW_DEV_COREDUMP=y
CONFIG_DEV_COREDUMP=y
+CONFIG_DEBUG_DRIVER=y
+CONFIG_DEBUG_DEVRES=y
+# CONFIG_DEBUG_TEST_DRIVER_REMOVE is not set
# CONFIG_TEST_ASYNC_DRIVER_PROBE is not set
CONFIG_GENERIC_CPU_AUTOPROBE=y
CONFIG_REGMAP=y
@@ -1695,6 +1700,7 @@ CONFIG_I2C_SLAVE=y
# CONFIG_I3C is not set
CONFIG_SPI=y
+# CONFIG_SPI_DEBUG is not set
CONFIG_SPI_MASTER=y
CONFIG_SPI_MEM=y
@@ -1760,6 +1766,7 @@ CONFIG_PINMUX=y
CONFIG_GENERIC_PINMUX_FUNCTIONS=y
CONFIG_PINCONF=y
CONFIG_GENERIC_PINCONF=y
+CONFIG_DEBUG_PINCTRL=y
# CONFIG_PINCTRL_AMD is not set
# CONFIG_PINCTRL_MCP23S08 is not set
CONFIG_PINCTRL_SINGLE=y
@@ -1773,6 +1780,7 @@ CONFIG_GPIOLIB=y
CONFIG_GPIOLIB_FASTPATH_LIMIT=512
CONFIG_OF_GPIO=y
CONFIG_GPIOLIB_IRQCHIP=y
+CONFIG_DEBUG_GPIO=y
# CONFIG_GPIO_SYSFS is not set
#
@@ -2184,6 +2192,7 @@ CONFIG_DRM=y
CONFIG_DRM_MIPI_DSI=y
# CONFIG_DRM_DP_AUX_CHARDEV is not set
# CONFIG_DRM_DEBUG_MM is not set
+# CONFIG_DRM_DEBUG_SELFTEST is not set
CONFIG_DRM_KMS_HELPER=y
CONFIG_DRM_KMS_FB_HELPER=y
CONFIG_DRM_FBDEV_EMULATION=y
@@ -3992,39 +4001,53 @@ CONFIG_SBITMAP=y
# printk and dmesg options
#
CONFIG_PRINTK_TIME=y
-# CONFIG_PRINTK_CALLER is not set
-CONFIG_CONSOLE_LOGLEVEL_DEFAULT=7
-CONFIG_CONSOLE_LOGLEVEL_QUIET=4
-CONFIG_MESSAGE_LOGLEVEL_DEFAULT=4
+CONFIG_PRINTK_CALLER=y
+CONFIG_CONSOLE_LOGLEVEL_DEFAULT=15
+CONFIG_CONSOLE_LOGLEVEL_QUIET=15
+CONFIG_MESSAGE_LOGLEVEL_DEFAULT=7
+# CONFIG_BOOT_PRINTK_DELAY is not set
# end of printk and dmesg options
#
# Compile-time checks and compiler options
#
+# CONFIG_DEBUG_INFO is not set
CONFIG_ENABLE_MUST_CHECK=y
CONFIG_FRAME_WARN=1024
# CONFIG_STRIP_ASM_SYMS is not set
+# CONFIG_READABLE_ASM is not set
# CONFIG_DEBUG_FS is not set
# CONFIG_HEADERS_INSTALL is not set
CONFIG_OPTIMIZE_INLINING=y
# CONFIG_DEBUG_SECTION_MISMATCH is not set
CONFIG_SECTION_MISMATCH_WARN_ONLY=y
+# CONFIG_DEBUG_FORCE_WEAK_PER_CPU is not set
# end of Compile-time checks and compiler options
# CONFIG_MAGIC_SYSRQ is not set
-# CONFIG_DEBUG_KERNEL is not set
+CONFIG_DEBUG_KERNEL=y
+CONFIG_DEBUG_MISC=y
#
# Memory Debugging
#
# CONFIG_PAGE_EXTENSION is not set
+# CONFIG_DEBUG_PAGEALLOC is not set
+# CONFIG_PAGE_OWNER is not set
# CONFIG_PAGE_POISONING is not set
# CONFIG_DEBUG_RODATA_TEST is not set
+# CONFIG_DEBUG_OBJECTS is not set
# CONFIG_SLUB_DEBUG_ON is not set
# CONFIG_SLUB_STATS is not set
CONFIG_HAVE_DEBUG_KMEMLEAK=y
+# CONFIG_DEBUG_KMEMLEAK is not set
+# CONFIG_DEBUG_STACK_USAGE is not set
+# CONFIG_DEBUG_VM is not set
CONFIG_ARCH_HAS_DEBUG_VIRTUAL=y
+# CONFIG_DEBUG_VIRTUAL is not set
CONFIG_DEBUG_MEMORY_INIT=y
+# CONFIG_DEBUG_PER_CPU_MAPS is not set
+# CONFIG_DEBUG_HIGHMEM is not set
CONFIG_CC_HAS_KASAN_GENERIC=y
CONFIG_KASAN_STACK=1
# end of Memory Debugging
@@ -4032,34 +4055,69 @@ CONFIG_KASAN_STACK=1
CONFIG_ARCH_HAS_KCOV=y
CONFIG_CC_HAS_SANCOV_TRACE_PC=y
# CONFIG_KCOV is not set
+# CONFIG_DEBUG_SHIRQ is not set
#
# Debug Lockups and Hangs
#
+# CONFIG_SOFTLOCKUP_DETECTOR is not set
+# CONFIG_DETECT_HUNG_TASK is not set
+# CONFIG_WQ_WATCHDOG is not set
# end of Debug Lockups and Hangs
# CONFIG_PANIC_ON_OOPS is not set
CONFIG_PANIC_ON_OOPS_VALUE=0
CONFIG_PANIC_TIMEOUT=0
+CONFIG_SCHED_DEBUG=y
+# CONFIG_SCHEDSTATS is not set
+# CONFIG_SCHED_STACK_END_CHECK is not set
# CONFIG_DEBUG_TIMEKEEPING is not set
+CONFIG_DEBUG_PREEMPT=y
#
# Lock Debugging (spinlocks, mutexes, etc...)
#
CONFIG_LOCK_DEBUGGING_SUPPORT=y
+# CONFIG_PROVE_LOCKING is not set
+# CONFIG_LOCK_STAT is not set
+# CONFIG_DEBUG_RT_MUTEXES is not set
+# CONFIG_DEBUG_SPINLOCK is not set
+# CONFIG_DEBUG_MUTEXES is not set
+# CONFIG_DEBUG_WW_MUTEX_SLOWPATH is not set
+# CONFIG_DEBUG_RWSEMS is not set
+# CONFIG_DEBUG_LOCK_ALLOC is not set
+# CONFIG_DEBUG_ATOMIC_SLEEP is not set
+# CONFIG_DEBUG_LOCKING_API_SELFTESTS is not set
+# CONFIG_LOCK_TORTURE_TEST is not set
# CONFIG_WW_MUTEX_SELFTEST is not set
# end of Lock Debugging (spinlocks, mutexes, etc...)
# CONFIG_STACKTRACE is not set
# CONFIG_WARN_ALL_UNSEEDED_RANDOM is not set
+# CONFIG_DEBUG_KOBJECT is not set
CONFIG_DEBUG_BUGVERBOSE=y
+# CONFIG_DEBUG_LIST is not set
+# CONFIG_DEBUG_PLIST is not set
+# CONFIG_DEBUG_SG is not set
+# CONFIG_DEBUG_NOTIFIERS is not set
+# CONFIG_DEBUG_CREDENTIALS is not set
#
# RCU Debugging
#
+# CONFIG_RCU_PERF_TEST is not set
+# CONFIG_RCU_TORTURE_TEST is not set
CONFIG_RCU_CPU_STALL_TIMEOUT=21
+# CONFIG_RCU_TRACE is not set
+# CONFIG_RCU_EQS_DEBUG is not set
# end of RCU Debugging
+# CONFIG_DEBUG_WQ_FORCE_RR_CPU is not set
+# CONFIG_DEBUG_BLOCK_EXT_DEVT is not set
+# CONFIG_CPU_HOTPLUG_STATE_CONTROL is not set
+# CONFIG_NOTIFIER_ERROR_INJECTION is not set
+# CONFIG_FAULT_INJECTION is not set
+# CONFIG_LATENCYTOP is not set
CONFIG_HAVE_FUNCTION_TRACER=y
CONFIG_HAVE_FUNCTION_GRAPH_TRACER=y
CONFIG_HAVE_DYNAMIC_FTRACE=y
@@ -4072,7 +4130,11 @@ CONFIG_TRACING_SUPPORT=y
CONFIG_RUNTIME_TESTING_MENU=y
# CONFIG_TEST_LIST_SORT is not set
# CONFIG_TEST_SORT is not set
+# CONFIG_BACKTRACE_SELF_TEST is not set
+# CONFIG_RBTREE_TEST is not set
# CONFIG_REED_SOLOMON_TEST is not set
+# CONFIG_INTERVAL_TREE_TEST is not set
+# CONFIG_PERCPU_TEST is not set
# CONFIG_ATOMIC64_SELFTEST is not set
# CONFIG_TEST_HEXDUMP is not set
# CONFIG_TEST_STRING_HELPERS is not set
@@ -4105,17 +4167,30 @@ CONFIG_RUNTIME_TESTING_MENU=y
# CONFIG_BUG_ON_DATA_CORRUPTION is not set
# CONFIG_SAMPLES is not set
CONFIG_HAVE_ARCH_KGDB=y
+# CONFIG_KGDB is not set
# CONFIG_UBSAN is not set
CONFIG_UBSAN_ALIGNMENT=y
CONFIG_ARCH_HAS_DEVMEM_IS_ALLOWED=y
# CONFIG_STRICT_DEVMEM is not set
+# CONFIG_ARM_PTDUMP_DEBUGFS is not set
# CONFIG_DEBUG_WX is not set
# CONFIG_UNWINDER_FRAME_POINTER is not set
CONFIG_UNWINDER_ARM=y
CONFIG_ARM_UNWIND=y
-# CONFIG_DEBUG_USER is not set
-CONFIG_DEBUG_LL_INCLUDE="mach/debug-macro.S"
+CONFIG_DEBUG_USER=y
+CONFIG_DEBUG_LL=y
+CONFIG_STM32MP1_DEBUG_UART=y
+# CONFIG_DEBUG_ICEDCC is not set
+# CONFIG_DEBUG_SEMIHOSTING is not set
+# CONFIG_DEBUG_LL_UART_8250 is not set
+# CONFIG_DEBUG_LL_UART_PL01X is not set
+CONFIG_DEBUG_STM32_UART=y
+CONFIG_DEBUG_LL_INCLUDE="debug/stm32.S"
+CONFIG_DEBUG_UART_PHYS=0x40010000
+CONFIG_DEBUG_UART_VIRT=0xfe010000
+CONFIG_DEBUG_UNCOMPRESS=y
CONFIG_UNCOMPRESS_INCLUDE="debug/uncompress.h"
+CONFIG_EARLY_PRINTK=y
# CONFIG_PID_IN_CONTEXTIDR is not set
# CONFIG_CORESIGHT is not set
# end of Kernel hacking
Change to the stm32mp15xx-dkx.dtsi
index df96874c1f..685a82161c 100644
--- a/arch/arm/boot/dts/stm32mp15xx-dkx.dtsi
+++ b/arch/arm/boot/dts/stm32mp15xx-dkx.dtsiold
@@ -260,10 +260,10 @@
};
};
-&i2c2 {
+&i2c4 {
pinctrl-names = "default", "sleep";
- pinctrl-0 = <&i2c2_pins_a>;
- pinctrl-1 = <&i2c2_pins_sleep_a>;
+ pinctrl-0 = <&i2c4_pins_a>;
+ pinctrl-1 = <&i2c4_pins_sleep_a>;
i2c-scl-rising-time-ns = <185>;
i2c-scl-falling-time-ns = <20>;
clock-frequency = <400000>;
Complete bootlog (mmc not configured)
Boot log attached.
I am probably missing something trivial. Thanks for the help!
BR
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-01-13 1:23 AM
Sorry, my reply is on the wrong level.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-01-13 1:28 AM
Hi @Community member​
Can you share your kernel DT ?
I'm also still interesting to get TF-A and Uboot traces ( prior to kernel traces )
Thx,
Olivier
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-01-13 1:44 AM
Sure, again thank you.
I use https://github.com/STMicroelectronics/linux/blob/v5.4-stm32mp/arch/arm/boot/dts/stm32mp157a-dk1.dts with the modification to the i2c4 -> i2c2 as shown above for the stm32mp15xx-dkx.dtsi.
For the TF-A and Uboot I have my more complete DT (Ethernet + MMC + PMIC on I2C2), thus dirty.
Here is the traces
NOTICE: CPU: STM32MP157CAC Rev.B
NOTICE: Model: STMicroelectronics STM32MP157A-DK1 Discovery Board
INFO: Reset reason (0x15):
INFO: Power-on Reset (rst_por)
INFO: PMIC version = 0x20
INFO: Using USB
INFO: Instance 2
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.2-r2.1(debug):v2.2-stm32mp-r2.1-1-g048a4dbf-dirty
NOTICE: BL2: Built : 01:15:32, Jan 8 2021
INFO: Using crypto library 'stm32_crypto_lib'
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-DDR3L 16bits 533000Khz
INFO: Memory size = 0x20000000 (512 MB)
INFO: BL2 runs SP_MIN setup
INFO: BL2: Loading image id 4
INFO: Loading image id=4 at address 0x2ffeb000
INFO: Image id=4 loaded: 0x2ffeb000 - 0x2ffff000
INFO: BL2: Loading image id 5
INFO: GETSTATUS :
INFO: DFU_STATE_IDLE
INFO: UPLOAD :
INFO: Phase ID : 0
INFO: address 0x2ffe76b0
INFO: GETSTATUS :
INFO: DFU_STATE_IDLE
INFO: GETSTATUS :
INFO: DFU_STATE_IDLE
INFO: UPLOAD :
INFO: Phase ID : 0
INFO: address 0x2ffe76b0
INFO: GETSTATUS :
INFO: DFU_STATE_IDLE
INFO: Start Download partition 0 to address 0xc0000000 length 0
INFO: USB : DFU : end of download partition : 0
INFO: Loading image id=5 at address 0xc0100000
INFO: GETSTATUS :
INFO: DFU_STATE_IDLE
INFO: UPLOAD :
INFO: Phase ID : 3
INFO: address 0x2ffe76b0
INFO: GETSTATUS :
INFO: DFU_STATE_IDLE
INFO: receive request 6
INFO: GETSTATUS :
INFO: DFU_STATE_IDLE
INFO: UPLOAD :
INFO: Phase ID : 3
INFO: address 0x2ffe76b0
INFO: GETSTATUS :
INFO: DFU_STATE_IDLE
INFO: usb_partition_size: partition size : 0xd3370
INFO: Start Download partition 3 to address 0xc0100000 length 865136
INFO: USB : DFU : end of download partition : 3
INFO: GETSTATUS :
INFO: DFU_STATE_IDLE
INFO: UPLOAD :
INFO: Phase ID : 0
INFO: address 0xffffffff
INFO: Send detach request
INFO: GETSTATUS :
INFO: DFU_STATE_IDLE
INFO: Receive Detach
INFO: Image id=5 loaded: 0xc0100000 - 0xc01d3370
WARNING: Skip signature check (header option)
NOTICE: ROTPK is not deployed on platform. Skipping ROTPK verification.
NOTICE: BL2: Booting BL32
INFO: Entry point address = 0x2ffeb000
INFO: SPSR = 0x1d3
NOTICE: SP_MIN: v2.2-r2.1(debug):v2.2-stm32mp-r2.1-1-g048a4dbf-dirty
NOTICE: SP_MIN: Built : 01:15:32, Jan 8 2021
INFO: ARM GICv2 driver initialized
INFO: Set calibration timer to 60 sec
INFO: stm32mp IWDG1 (12): Secure
INFO: ETZPC: CRYP1 (9) could be non secure
INFO: SP_MIN: Initializing runtime services
INFO: SP_MIN: Preparing exit to normal world
U-Boot 2020.01-stm32mp-r2.1-00004-g94171b1205-dirty (Jan 08 2021 - 18:15:58 +0100)
CPU: STM32MP157CAC Rev.B
Model: ***
Board: stm32mp1 in trusted mode (st,stm32mp157a-dk1)
DRAM: 512 MiB
Clocks:
- MPU : 650 MHz
- MCU : 208.878 MHz
- AXI : 266.500 MHz
- PER : 24 MHz
- DDR : 533 MHz
Fastboot key pressed, STM32Programmer key pressed, entering download mode...
WDT: Started with servicing (32s timeout)
NAND: 0 MiB
MMC: STM32 SD/MMC: 2
In: serial
Out: serial
Err: serial
Net: eth0: ethernet@5800a000
STM32MP>
STM32MP> run get_kernel_dt_from_tftp
ethernet@5800a000 Waiting for PHY auto negotiation to complete... done
Using ethernet@5800a000 device
TFTP from server server_ip; our IP address is client_ip
Filename 'zImage'.
Load address: 0xc2000000
Loading: *#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
###############
640.6 KiB/s
done
Bytes transferred = 4068776 (3e15a8 hex)
Using ethernet@5800a000 device
TFTP from server server_ip; our IP address is client_ip
Filename 'stm32mp157a-dk1.dtb'.
Load address: 0xc4000000
Loading: *#####################
3.1 MiB/s
done
Bytes transferred = 103087 (192af hex)
Kernel image @ 0xc2000000 [ 0x000000 - 0x3e15a8 ]
## Flattened Device Tree blob at c4000000
Booting using the fdt blob at 0xc4000000
Loading Device Tree to cffe3000, end cffff2ae ... OK