User Activity

Hello, I'm currently working with a STM32MP157D-DK1 Development Board with 4GB DDR3L. I populated the board with a prebuild openstlinux 6.1 build like discribed in a guide in the ST wiki.When checking the total memory i unfortunatly only get 407MB th...
Hello, I currently working with a STM32MP157D-DK1 Development Board. I populated the board with a prebuild openstlinux 6.1 build. A SSH connection via console is successful.To get the M4 microcontroller running I was able to build a .elf file from th...
Hey,I'm using the Timer 2 in Encoder Mode TI1 and TI2. The Trigger Output of the Timer is set to Master/Slave Mode Enabled and the Trigger Event is set to Compare Pulse (OC1).As far as I know: This Timer will fire an internal interrupt via TRGO every...
Hey,I'm using a Nucleo-F446RE and the STM32 Cube IDE.I want to start the Timer3 with a changing Edge at a GPIO Pin. Then the Timer should count till another GPIO has a changing Edge aswell. Now the timer should be disabled and the counter should be s...
Kudos given to