User Activity

Hello,For STM32G4 Rev Y:Errata 2.7.3Wrong ADC result if conversion done late after calibration or previous conversion DescriptionThe result of an ADC conversion done more than 1 ms later than the previous ADC conversion or ADC calibration might be in...
Hello,I would like to test the behaviour of STM32G4 MCU timers on exceptions. The SYSCFG register has several options for timer break. The HAL library provides the following macros to activate these options:__HAL_SYSCFG_BREAK_ECC_LOCK();__HAL_SYSCFG_...
Hello,I have a few questions about X-CUBE-MEMS as following:Can we run multiple algorithms (MotionFX, MotionDI, MotionTilt etc) on the same platform simultaneously using the same input data? I would like to make performance comparision between algori...
Hello,I need to use dual MEMS (ISM330DHCX) and MCU in my application for redundancy. Each MEMS is connected to a different MCU with independent supply. The data collected from sensors will be crossed checked if within a predefined tolerance. I think ...
Kudos from