BLUENRG-M2SA is my processor. I am starting a gpio toggle to test it out. It compiles normally in Keil and Atollic. It only appears to use Keil program even when attolic is the programmer. The device will enter debug mode in Attollic how ever it ...
I am trying to find out how to set up this as a master processor. I am trying to find out how to program it. Is an Stlink/V2 acceptable to flash it. I am not seeing a pinout on BLUENRG-M2SA for SWDIO and SWCLK. It is not supported by Cubemx ...
I use stm32 eclipse to add two folders in a folder named drivers. One is for my .c files named src and the second is inc for my header files. The .c can not seem to read the header files when called up on. I am new to this so the answer should be ...
I am needing a 50mA current so I change ISET to 37.4K. I changed the OVAP with 100k R1 and R to 4.12k. When I apply 5V to both PWM and EN the chip it fried my board. I am trying to find out what I did wrong before I continue. 3LEDS are being driven. ...
Posted on March 22, 2016 at 18:20Does this kit require a BDM to program the STM32F429ZIT6. Or does it work through the USB? I am new to ST products and what kind of tools do I need to use to program the device.
I am confused on the solution . I go to project->properties> C/C++Build I do not see MCU GCC Compiler->Dialect->Other dialect flag any where on the GUI