User Activity

Hello there,I don't know if I can call this a bug, but it shouldn't happen at all.Thing goes like this: I have a STM32G071, I enabled UCPD1 and 2, also CMSIS, USBPD library in CubeMXI generated code for SW4STM32, I write my custom board code in usbpd...
Dear members,This is actually a follow up question to my last one STM32G071 UCPD library bug or my problem, but instead of digging deeper and deeper to an already well answered question, and probably out of topic too, I guess I better start a new one...
Hello there, I have a custom board with STM32G071CB for USB Type C PD Source, dual port, RTOS, configured with CubeMX 5.3.0, after writing code on usbpd_dpm_user.c and start debugging, I suspected there are 2+1 strange behavior so I hope somebody can...