User Activity

I'm using the STM32F769-DISC0 development board and am utilizing the DWT->CYCCNT to calculate cpu load as well as using it as a high speed timer that runs at the clock frequency. When the debugger is plugged in, it functions fine. However, with the d...
Specifically for the SPC58 -- although it looks like the 56/57 share the same registers. I've reviewed the documentation for the time base registers (TBU/TBL) and have made an attempt to enable it. Leaving the timebase clock (SEL_TBCLK) at the proces...
I had a functioning TCP/IP application I am trialing on the SPC58EC-DISP discovery board using DHCP. SPC5Studio pulled updates and is not forcing me to migrate to the latest RLA (1.8.2.20200908161300) which breaks some network code -- this was fixed....