User Activity

I see that the page related to the installation on java is still under construction on the wiki, but I urgently want to install jre and want help in doing so.I am using st-example-image-qt for my project and I need to add java to it, I have already a...
I am trying to flash a 32gb sd card with stlinux for STM32MP157C-DK2 using the guide at https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157C-DK2/Let%27s_start/Populate_the_target_and_boot_the_image The SD card that came with ...
I want to build a BLE repeater using the ​spbtle-rf0 module, I am using the x-nucleo-idb05a1 expansion board for the development. I saw that a radio driver is available for bluenrg-1 and bluenrg-2 modules but couldn't find it for spbtle-rf0 which is ...
Kudos from