2020-10-01 2:38 AM
I see that the page related to the installation on java is still under construction on the wiki, but I urgently want to install jre and want help in doing so.
I am using st-example-image-qt for my project and I need to add java to it, I have already added other packages like python, etc. using the IMAGE_INSTALL_append = python3, but when I add openjdk-7-jre in it after adding the meta-java layer, it gives an error that x11 is required in DISTRO_FEATURES.
Please help me fix this.
Thanks and Regards
2020-10-06 8:33 AM
Hi @Puranjay Mohan ,
Yes wiki page is currently in final review process and should be public very soon.
In the meantime, find below extract of main info :
JAVA for Linux-based system for embedded system is available as a meta data in Yocto project.
PC >git clone git://git.yoctoproject.org/meta-javaDepending on the Yocto release, select the right branch. (example : branch dunfell for the ecosystem release v2.0.0
The last commit tested is cf9604a4789801d9dfb0cb8ca134ff04b42ae161 : openjdk-8: remove -Werror
PC $>cd meta-java
PC $>git checkout remotes/origin/dunfell If not done, setup your build environment:
PC $> cd [your STM32MP1 Distribution path]
PC $> source ./meta-st/script/envsetup.sh
(Select for the DISTRO openstlinux-weston and for MACHINE stm32mp1)Add the meta layer in your yocto environment :
PC $> cd [your STM32MP1 Distribution path]/build-openstlinuxweston-stm32mp1
PC $> bitbake-layers add-layer [your STM32MP1 Distribution path]/meta-st/meta-javaDefine at least the following variables in your local.conf file.
([your STM32MP1 Distribution path]/build-openstlinuxweston-stm32mp1/conf/local.conf)
#Possible provider: cacao-initial-native and jamvm-initial-native
PREFERRED_PROVIDER_virtual/java-initial-native = "cacao-initial-native"
#Possible provider: cacao-native and jamvm-native
PREFERRED_PROVIDER_virtual/java-native = "jamvm-native"
#Optional since there is only one provider for now
PREFERRED_PROVIDER_virtual/javac-native = "ecj-bootstrap-native"Include in your image the openjdk-8 component
PC $> cd [your STM32MP1 Distribution path]/meta-st/meta-st-openstlinux/recipes-st/imagesEdit the file st-image-weston.bb and add the following line under CORE_IMAGE_EXTRA_INSTALL
openjdk-8 \
openjdk-8-demo \Build the image
PC $> cd [your STM32MP1 Distribution path]/build-openstlinuxweston-stm32mp1
PC $> bitbake st-image-westonHope it help,
Olivier