If I use the standalone mx ( which is the same version as the one in IDE though ) It works, well, almost...The generated b_l475e_iot01a1_bus.c cannot be compiled, because it cannot find the configured pins, which are defined in main.hInlcuding main.h...
Hi Silvio,I use Cube IDE ( from "About" page):STM32CubeIDE Version: 1.3.1 Build: 6291_20200406_0752 (UTC)STM32CubeMX 5.6.1.202004052303 com.st.stm32cube.common.feature.mxI created the project from scratch as follows:new STM32 projectI select the boar...