Receiving TCP stream that spans two packets fails after several seconds. Pings still work. The STM32F7 replies to the receive stream with duplicate ACK'sThe TCP stream does not recover.Ethernet Receive Logic Review using STM32Cube_FW_H7_V1.3.2/Proj...
Posted on July 31, 2017 at 22:35In STM32Cube_FW_F7_V1.7.0/Projects/STM32746G-Discovery/Examples/SPI/SPI_FullDuplex_ComDMA example shows a simple DMA transfer with data cache on. How can aRxBuffer buffer can be updated correctly without a region def...
Posted on May 19, 2017 at 01:02Issue:USB Core issing interrupt at a rate of 8.65us causing high CPU loading.Software/Chip:Using USB Host/CDC from STM32Cube V1.15 on a STM32F429 board. USB interrupt sources:- SOF Interrupts (It is not needed for CD...
Posted on July 06, 2016 at 16:22Running the install SetupSTM32CubeMX-4.15.1.linuxcrashes. OS: Ubuntu 16.04LTS 64 Bitjava version:java -versionopenjdk version ''9-internal''OpenJDK Runtime Environment (build 9-internal+0-2016-04-14-195246.buildd.src)...
Posted on March 27, 2015 at 17:38Compiled and downloaded the FatFS_USBDisk to the board and it verified the file is written to the USB flash disk and the LED is green. Also, reconnected several times and validate the LED 3 goes green each time. ...
Posted on August 01, 2017 at 15:07After looking at the code more, the reason why this works once is aRxBuffer is not in the data cache since it has not been read. I would hope the examples for the F7/H7 would be updated to reflect cache issues, not...