cancel
Showing results for 
Search instead for 
Did you mean: 

stm32cubemx Ubuntu 16.04 LTS 64 Bit crash

Tim Michals
Associate II
Posted on July 06, 2016 at 16:22

Running the install SetupSTM32CubeMX-4.15.1.linux

crashes. 

OS: Ubuntu 16.04LTS 64 Bit

java version:

java -version

openjdk version ''9-internal''

OpenJDK Runtime Environment (build 9-internal+0-2016-04-14-195246.buildd.src)

OpenJDK 64-Bit Server VM (build 9-internal+0-2016-04-14-195246.buildd.src, mixed mode)

Attached is crash log

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Posted on May 19, 2017 at 01:04

Yes, it does.  Thank you issue resolved.

View solution in original post

6 REPLIES 6
Nesrine M_O
Lead II
Posted on July 13, 2016 at 15:07

Hi michals.tim,

I have an issue to open your crash log.Could you please reattach it? 

-Syrine-

rchrdlyon1
Associate II
Posted on July 14, 2016 at 17:09

I have a similar problem with the same operating system. When I try:

cd to directory where the file SetupSTM32CubeMX-4.15.1.linux is located

$ sudo ./SetupSTM32CubeMX-4.15.1.linux

The installer runs but always generates the following message:

sudo: unable to execute ./SetupSTM32CubeMX-4.15.1.linux: No such file or directory

Tried the default openjdk as well as oracle java.

The last version of of the installer that worked was SetupSTM32CubeMX-4.13.0.linux with oracle java. Later versions do not. Hopefully one day this problem will resolved.

Regards ...

rchrdlyon1
Associate II
Posted on July 14, 2016 at 18:22

sudo java -jar SetupSTM32CubeMX-4.15.1.exe -console

seems to work. STM32CubeMX is working on default openjdk supplied with ubuntu.

stm32cube-t
ST Employee
Posted on July 21, 2016 at 12:11

Dear all,

We do not reproduce your issue.

Please note STM32CubeMX on Linux is a 32 bit application. Do you confirm that you have 32 bit compliant packages installed on your Linux 64 bit?

The tool also requires: java 1.7.0_45 or later.

Best regards 

Sirma Siang
ST Employee
Posted on February 02, 2017 at 12:05

Hello All,

CubeMX-4.19 with oracle java version 1.8.0_121, on Ubuntu 64 bits has been tested.

IT works well.

I was able to install, launch and creates a project.

Has this thread was long ago, I guess everything has been fixed since.

Kind regards

Sirma

Posted on May 19, 2017 at 01:04

Yes, it does.  Thank you issue resolved.