cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 Discovery USB Host example (Beagle USB 480)

Tim Michals
Associate II
Posted on March 27, 2015 at 17:38

Compiled and downloaded the FatFS_USBDisk to the board and it verified the file is written to the USB flash disk and the LED is green.  Also, reconnected several times and validate the LED 3 goes green each time.

 

Attempting to trace the USB traffic using a Beagle USB 480, no traffic is captured, it just shows <Host disconnected>  But, the example works with out an issue. Is there a clocking issue?

(The example works when the USB flash stick is connected to the Beagle USB 480 also)

Verified the USB Beagle is working and able to capture traffic.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0